Technical FAQs

Ask a Question

How to install a 30mm 9001K/9001SK operator

Product Line:
9001K/9001SK style Operators

Resolution:
1. Remove the mounting collar from the button.
2. Remove the clear and metal washer.
3. Discard one rubber washer from the button.
4. Slide the button through the indide of the panel so that it is facing outwards.
5. Reattach the clear and metal washer from the outside of the enclosure.
6. Use the Mounting collar to attach the button to the enclosure.
Was this helpful?
What can we do to improve the information ?