Technical FAQs

Ask a Question

What is the latest firmware version for the Altivar 61/71 Modbus Plus Card?

Issue:
What is the latest firmware version for the Altivar 61/71 Modbus Plus Card?

Product Line:
ATV61/71

Environment:
All serial numbers for ATV61/71

Cause:
N/A

Resolution:
The part number for the card is VW3A3302
The latest version is V1.1IE03.
Was this helpful?
What can we do to improve the information ?