Technical FAQs

Ask a Question

What are the replacement fuses for the RAM DBS board set?

Issue:
What are part numbers for the RAM DBS board set fuses?

Product Line:
RAM DBS and DBS II

Environment:
All models

Cause:
Blown fuses

Resolution:
The board set has 2 fuses:
FU-0081 is the .25A FU1 fuse.
FU-0082 is the 5A FU2 fuse.

Contact RAM Industries customer service at 800-999-8183, option 4.

Was this helpful?
What can we do to improve the information ?