Technical FAQs

Ask a Question

What are the replacement contactors for the RAM DBS II starters?

Issue:
What are the replacement contactors for the RAM DBS II starters?

Product Line:
RAM DBS II

Environment:
All models

Cause:
Chassis shorting contactor failed.

Resolution:
The RAM DBS II chassis includes a shorting contactor that can be replaced.  Due to periodic design changes, it is important to look at the existing contactor type before a replacement is ordered.  See the attached file for info on the current design.
Was this helpful?
What can we do to improve the information ?