Technical FAQs

Ask a Question

How do you wire in a damper circuit on the S-Flex SFD212 enclosed drives without a bypass and with old P24 to F control start circuit?

Issue:
How do you wire in a damper circuit on the S-Flex  SFD212 enclosed drives without a bypass and with old P24 to F control start circuit?

Product Line:
S-Flex 212 with old wiring control circuit P24 and F.

Environment:
All 

Cause:
Wants to add in a damper option to an enclosed SFD212 drive without bypass and old P24 and F control start. 

Resolution:
Customer will need to use the auto start dry contact  to feed their solenoid coil.  This will start the process of opening the damper.  Once the damper is open we need a limit switch or sensor to see feedback to the drives P24 and F to start up the drive. 
Was this helpful?
What can we do to improve the information ?