Technical FAQs

Ask a Question

What are notable physical differences between the old and new RAM DBS board set?

Issue:
What are notable physical differences between the old and new RAM DBS board set?
 
Product Line:
DBS and DBS II
 
Environment:
All models
 
Cause:
Troubleshoot or replace
 
Resolution:
The board set design change occurred 10/18/2004.
The most prominent differences are:
green vs blue circuit boards
one fuse vs 2 fuses
CT connector style
reset switch large red vs small black
See the below photos.


 
Was this helpful?
What can we do to improve the information ?