Technical FAQs

Ask a Question

Does the drive need to be re-programmed if the VW3A1101 HMI keypad is replaced?

Issue:
Program the drive

Product Line:
Part number VW3A1101
ATV212, ATV61, ATV71, ATV32, ATV31, ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
No, re-programming is required.  The program is saved in an EEPROM in the drive.
Was this helpful?
What can we do to improve the information ?