Technical FAQs

Ask a Question

Are Powerpact breakers available with 50 degrees C calibration?

Product Line:
Powerpact H and J frame

Resolution:
Add "CA" suffix to H- or J-frame thermal magnetic circuit breaker catalog numbers for 50 degrees C calibration.  The breaker will not be UL Listed with 50C calibration.
See Supplemental & Obsolescence Digest 177, page 3-15.
Was this helpful?
What can we do to improve the information ?