Technical FAQs

Ask a Question

What does the rotating arrows indicate on the ATV66 drives keypad display?

Issue:
What does the rotating arrows indicate on the ATV66 drives keypad display?

Product Line:
Altivar ATV66 drive

Environment:
All 

Cause:
Needs to know why the drive does not have a output when the status screen shows a rotating clockwise arrow.

Resolution:
The rotating arrow indicates that the motor is turning and in what direction. 
The rotating arrow should indicate that the motor is turning. if the motor is not turning then get a meter and check the output voltage to see if there is any voltage coming out of the drive. 
Was this helpful?
What can we do to improve the information ?