Technical FAQs

Ask a Question

Are the test and mute buttons, LED's, or terminal blocks, available as repair parts for the IG2000PG1, IG2000PG2, IG2000CBMG2 or IG2000CBMG4 medical remote indicators?

Issue:
Are the test and mute buttons, LED's, or terminal blocks, available as repair parts for the IG2000PG1, IG2000PG2,  IG2000CBMG2 or IG2000CBMG4 medical remote indicators?

Product Line:
Medical Remote Indicators

Environment:
IG2000

Cause:
Maintenance

Resolution:
No, There are no repair parts available for the IG2000PG1, IG2000PG2, IG2000CBMG2 or IG2000CBMG4 remote indicators. These are sold as a complete unit. The flush mounting plate is also not available as a repair part.
Was this helpful?
What can we do to improve the information ?