Technical FAQs

Ask a Question

Is there a Remote Reset for the LR9D Solid State Overloads?

Issue:
Is there a remote reset mechansism for the LR9D overload relays?

Product Line:
IEC Overload Relays - GIC Product

Environment:
US Product

Cause:
Product Accessories

Resolution:
No, these units can only be reset via a through the door plunger type mechanism.
Was this helpful?
What can we do to improve the information ?