Technical FAQs

Ask a Question

Do the 8538 Combination starters in a NEMA 12/3R enclosure come with gasketing?

Issue:
Do the 8538 Combination starters with a NEMA 12/3R enclosure come with gasketing?

Product Line:
NEMA Starters and Contactors - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
Yes, these units are gasketed around the inside seal.
Was this helpful?
What can we do to improve the information ?