Technical FAQs

Ask a Question

Does an E-Flex enclosure come with an external speed potentiometer when ordered with the A07 option?

Issue:
Does an E-Flex enclosure come with an external speed potentiometer when ordered with the A07 option?

Product Line:
E-Flex

Environment:
All serial numbers for E-Flex

Cause:
N/A

Resolution:
No the E-Flex does not come with an external speed pot unless you are ordering the Nema 3r enclosure.
When ordering the A07 option with a Nema 1 or Nema 12/12K, the middle knob on the keypad mounted in front of the enclosure is used as the speed potentiometer.

 
Was this helpful?
What can we do to improve the information ?