Technical FAQs

Ask a Question

Are lugs included with the high horsepower Altivar drives?

Issue: 
Are lugs included with the high horsepower Altivar drives?

Product Line:
ATV61 ATV71 

Environment:
All 

Cause:
N/A 

Resolution:
Lugs are not include with high horsepower drives. 
 
Was this helpful?
What can we do to improve the information ?