Technical FAQs

Ask a Question

What is the replacement control/display unit for the RAM DBS II ?

Issue:
What is the replacement control/display unit for the RAM DBS II ?
 
Product Line:
DBS and DBS II
 
Environment:
All models
 
Cause:
Replacement
 
Resolution:
The control/display is part number RAM-400437-05. 
The DBS manual references the unit as a KL4.  Note that a KL4 is manufactured with different EEPROMs for different products.  The KL4 for a DBS or DBS II will have 400437-05 on a label on the backside of the unit.
 
Was this helpful?
What can we do to improve the information ?