Technical FAQs

Ask a Question

Do the LXD1 coils come with replacement springs?

Issue:
Do the LXD1 coils come with replacement springs?

Product Line:
IEC Coils - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
These coils do not come with replacement springs.  The springs are not available as a separate order item.  If spring replacement is necessary, a new contactor should be ordered instead.
Was this helpful?
What can we do to improve the information ?