Technical FAQs

Ask a Question

What are the NEMA starter voltage codes which correspond to transformer control?

Issue:
What are the NEMA starter voltage codes which correspond to transformer control?

Product Line:
NEMA Starters - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
These are the voltages codes currently in use
Primary Secondary Code
120/60 12/60 V88
120/60 24/60 V89
208/60 24/60 V90
208/60 120/60 V84
240/60 24/60 V82
240/60 120/60 V80
277/60 24/60 V94
277/60 120/60 V85
347/60 24/60 V93
347/60 120/60 V92
380/50 110/50 V95
480/60 24/60 V83
480/60 120/60 V81
480/60 240/60 V87
600/60 24/60 V91
600/60 120/60 V86
Specify Other Voltage   V99
Was this helpful?
What can we do to improve the information ?