Technical FAQs

Ask a Question

Will the process drive fit in an E-Flex?

Issue:
ATV630 dimensions

Product Line:
ATV630

Environment:
All models and serial numbers

Cause:
None

Resolution:
The process drives have different dimensions than the ATV61 drives so they will not fit in the same footprint.
Was this helpful?
What can we do to improve the information ?