Technical FAQs

Ask a Question

How to find the Micrologic Trip Unit firmware version

Product Line:
Micrologic P and H Trip Units

Resolution:
Do the following to find the firmware version of a Micrologic P or H Trip Unit (trip unit screen must be powered to have access to the menu):
(1) On the front of the trip unit, press the "wrench" button
(2) Scroll down to "Micrologic Setup", and press enter
(3) Scroll down to "Breaker Selection", and press enter
The firmware version is shown at the bottom of the screen (example: 2009AJ)
Was this helpful?
What can we do to improve the information ?