Technical FAQs

Ask a Question

What is the stud (bolt) size on the SA8LL,Lug Landing kit? 

Issue:
What is the stud (bolt) size on the SA8LL,Lug Landing kit?

Product Line:
Speed-D Service and Distribution Switchboards.

Environment:
Speed-D Switchboard Lug Landing Kit, SA8LL sold in the USA. 

Cause:
Need to know the size of the bolts (Keps nuts). 

Resolution: 
The keps nuts for the SA8LL Lug Landing kit are 1/2-13 tighten to  250-350 lb-in. 
Refer to page 22 of the 80244-812-08. See attached bulletin below.
Was this helpful?
What can we do to improve the information ?