Technical FAQs

Ask a Question

How to do a soft reboot on the Wiser Air thermostat?

Issue: 
How to do a soft reboot on the Wiser Air thermostat?

Product Line:
Wiser Air

Environment:
Maintenance

Cause: 
Thermostat malfunctioning 

Resolution:
Below are the steps to perform the soft reboot process. 

1. Locate the small hole on the bottom left side of the thermostat. 
2. Insert the end of paper clip into the hole holding it firmly for about 8 seconds.
3. After 8 seconds the screen will go black and the device will begin to reboot. 
Was this helpful?
What can we do to improve the information ?