Technical FAQs

Ask a Question

Is Wiser Air compatible with Communicating HVAC Systems?

Product Line:
Wiser Air thermostat
Resolution:
No. Wiser Air is simply on-off switches that are shorted to the (R) terminal 24Vac energizing the heating and cooling equipment. Communicating systems use a serial communications protocol to communicate across the wires between the HVAC system and the thermostat.

Was this helpful?
What can we do to improve the information ?