Technical FAQs

Ask a Question

Wiser Air controls the fan but not engaging the heat pump.

Wiser Air
Make sure that the wires are making good contact to the back plate and installed correctly. Refer to the wiring setup in the document attached. If the installation is ok, please contact Technical Support for further assistance.

Phone: 1-(855)-55-WISER
Monday - Friday: 8 AM-12 AM EST
Saturday - Sunday: 10 AM-7 PM EST

Was this helpful?
What can we do to improve the information ?