Technical FAQs

Ask a Question

How do you set up the ATV212 drive to run above 60hz?

Issue:
How do you set up the ATV212 drive to run above 60hz?

Product Line:
Altivar ATV212

Environment:
All 

Cause:
Wants to run the drive above 60hz. 

Resolution:
Programming setup example.
FH= 72hz
UL= 72hz

If you are using analog inputs you will need to scale the analog inputs. 
VIA speed control change F204 to 72hz
VIB speed control change F213 to 72hz
Was this helpful?
What can we do to improve the information ?