Technical FAQs

Ask a Question

What is Heat pump balance?

PRODUCT LINE:
Wiser Air
RESOLUTION:
Heat Pump Balance monitors how well your heat pump is working and the current weather forecast. This feature will keep the comfort of your home on colder days when the heat pump has trouble maintaining the set point. If Eco IQ is engaged the algorithm predicts how this feature best suites your lifestyle in the future. Listed below are the compressor and Aux heat lockout temperatures when in heating mode.
  • Above 50 degrees the thermostat will enable the Y terminal and disable the W terminal.
  • Below 47 degrees both the Y and W terminal are enabled.
  • Below 17 degrees the Y terminal is disabled and W terminal is enabled. Once back above 17 degrees the Y terminal will be re-enabled.
Was this helpful?
What can we do to improve the information ?