Technical FAQs

Ask a Question

Is there an illuminated version of the 9001SKR16

Issue
Is there an illuminated version of the 9001SKR16 or can it be illuminated ?

Product Line: 
9001K & 9001SK

Environment
Pushbuttons

Resolution
No. It was adopted from the 22mm series and it has an adapter to which you will attach the contact block. You cannot mount a Light Module to that adapter.
Was this helpful?
What can we do to improve the information ?