Technical FAQs

Ask a Question

What is the temperature accuracy of Wiser Air?

Product Line: Wiser Air 
Resolution: 
Control Accuracy: 1°F (0.5°C)
Cooling Setpoint Range: 48°F to 95°F (9°C to 35°C)
Heating Setpoint Range: 45.5°F to 92°F (7.5°C to 33°C)
Display Range: 40°F to 95°F (5°C to 35°C)
Remote Sensor Compatibility: 10k NTC, Type 2
Was this helpful?
What can we do to improve the information ?