Technical FAQs

Ask a Question

How to control my fan on Wiser Air.

PRODUCT LINE:
Wiser Air
RESOLUTION:
The fan can be turned on or controlled to circulate the air to create an even temperature across the house per hour. This feature works with systems that can control the fan separately from heating and cooling. These systems have a separate G wire to control the fan. To access the fan control follow the steps below: 
  • On the thermostat tap on Menu, System, then Modes.
  • Next to Fan Modes select you can select auto, cycle or on.
    • Auto mode will engage the fan when ever the thermostat calls for heating or cooling.
    • Fan cycle durations can be set to 15, 30, or 45 minutes per hour. 
    • On will run the fan continuously 
Was this helpful?
What can we do to improve the information ?