Technical FAQs

Ask a Question

How many heating and cooling stages does Wiser Air support?

Product Line:
Wiser Air thermostat
Wiser Air is compatible with up to 2 stages of heating and up to 2 stages of cooling. 
To see if Wiser is compatible visit and used Compatibility Checker.


Was this helpful?
What can we do to improve the information ?