Technical FAQs

Ask a Question

For an ATV71HD75N4 drive, If the optional flange mount kit is used, how much of the drive is in front of the flange kit (inside the cabinet)?

Issue:
For an ATV71HD75N4 drive, If the optional flange mount kit is used, how much of the drive is in front of the flange kit (inside the cabinet)?

Product Line:
ATV71

Environment:
ATV71HD75N4 with optional flange kit VW3A9509 installed.

Cause:
Information is not available in current literature.

Resolution:
105mm of the drive (4.2 inches) will remain inside the enclosure.   
Was this helpful?
What can we do to improve the information ?