Technical FAQs

Ask a Question

What is the heat loss of the FLEX58KD54N4?

What is the heat loss of the FLEX58KD54N4?
Issue: 
What is the heat loss of the FLEX58KD54N4?
 
Product Line:
FLEX58
 
Environment:
FLEX58KD54N4, FLEX58D54N4
 
Cause:
N/A
 
Resolution:
Power dissipated from the heat sink 509.4 Watts
Power dissipated from the Control board 167.6 Watts
Total power dissipated - 677 watts              
 
Was this helpful?
What can we do to improve the information ?