Technical FAQs

Ask a Question

Are the communication parameters stored in the Keypad

On the ATV61/71, are the communication parameters stored in the Keypad on the VW3A1101?
Issue: 
On the ATV61/71, are the communication parameters stored in the Keypad on the VW3A1101?
 
Product Line:
Altivar 71, altivar 71
 
Environment:
All serial numbers
 
Cause:
Communicaton parameters will not transfer from the keypad
 
Resolution:
No, the communication parameters are not stored to the keypad, the communication parameters are stored in the communication card.              
 
Was this helpful?
What can we do to improve the information ?