Technical FAQs

Ask a Question

My PID enabled ATV630 drive will not wake, even after a power cycle it is still in sleep mode.

Issue:
My PID enabled ATV630 drive will not wake, even after a power cycle it is still in sleep mode.

Product Line:
ATV630 process drives.

Environment:
All models, All serial numbers

Cause:
Unexpected drive behavior

Resolution:
The ATV630 series drive, when sleep mode is enabled, will remember that it was in sleep mode through a run command cycle, and through a power cycle.  In order for the drive to wake, it is necessary that the conditions programmed into the "wake" tab be met.
Was this helpful?
What can we do to improve the information ?