Technical FAQs

Ask a Question

What does the star (*) at end of the part number in SoMove references mean?

Issue:
What does the star (*) at end of the part number in SoMove references mean?

Product Line:
Variable Frequency Drives

Environment:
Applies to all VFDs

Cause:
Customer wants to know what does the * at the end of the part number when selecting a reference in SoMove mean

Resolution:
* is a wildcard character that is used to represent one or more characters.
It is used to reduce the list of references in SoMove.
There is many special versions of a drive, par ex.:
- drive without graphic terminal has a Z letter at the end of the reference,
- drive without DC choke has a D letter at the end of the reference,
etc.

These special versions are the same as standard versions, from SoMove perspective.
Was this helpful?
What can we do to improve the information ?