Technical FAQs

Ask a Question

How do I enable/ disable Eco IQ Modes on Wiser Air?

Product Line:
 
Wiser Air 
Resolution: 
In order to enable Eco IQ your Wiser Air thermostat must be synced to an account before utilizing this option. Please see the following steps below on how you can access your Eco IQ Modes. 
On the Thermostat:
  1. Tap on Menu. 
  2. Select System. 
  3. Select Modes.
  4. Then select your Eco IQ Mode.
On the Mobile App: 
  1. Tap on Menu. 
  2. Select Settings.
  3. Scroll down and tap on Eco IQ.
  4. Then select your Eco IQ Mode.
On the Website:
  1.  Click on the account name on the top right.
  2. Select Profile & Settings.
  3. Scroll down to Devices & Device Permissions.
  4. Click on the up arrow of the device that you want to modify.
  5.  Then select Eco IQ Settings.
Was this helpful?
What can we do to improve the information ?