Technical FAQs

Ask a Question

Will Wiser Air work with variable speed fan?

Issue:  
Is Wiser Air compatible with variable speed fan?
Product Line:
Wiser Air thermostat
Environment:
Applies to Wiser Air thermostats only.
Resolution:
Some variable speed systems utilize proprietary wire connections and communications. These systems have custom wiring configurations and need to be connected to thermostats that are made by the same equipment manufacturer to work at “peak performance” and offer full access to all their features. The Wiser Thermostat does not work with these systems.

For more information you can provide the brand and model number of your thermostat to our support email address wiser_support@schneider-electric.com
Was this helpful?
What can we do to improve the information ?