Technical FAQs

Ask a Question

Linking GV3 with LC1D for UL Type F Applications

Issue:
What piece/part is used to electrically and mechanically link the GV3P starters with the LC1D contactors to achieve the UL Type F combination SCCR ratings?

Product Line:
IEC Starters and Contactors - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
No linkage part was used between the two units for SCCR testing.  Each component was mounted separately and linked only by the wiring.   
 
Was this helpful?
What can we do to improve the information ?