Technical FAQs

Ask a Question

Are EX Transformers 30% more efficient than the TP1 ratings?

Issue:
Are EX Transformers 30% more efficient than the TP1 ratings?

Product Line:
Transformer

Environment:
EX transformers

Cause:
Product features and application

Resolution:
Yes. The Premium 30 units (the EPs that the EXs replaced) had a 30% improvement over the EE units (which met TP1)
Was this helpful?
What can we do to improve the information ?