Technical FAQs

Ask a Question

Where can you find the serial number on the ATV61 and ATV71 drives?

ATV71 Where can I find the drive serial number if the drive is not powered up?

Product Line:
Altivar 61
Altivar 71

All revisions

Requested in documentation

Look for the product label mounted externally on the side of the drive. The serial number is under the barcode. The number typically begins with 88 , 8B , EL, 6W.
If the drive is powered, use the LCD graphic keypad to navigate to the Drive Menu, 1.11 IDENTIFICATION.  The serial number is just beneath the MC sofware Version.
Was this helpful?
What can we do to improve the information ?