Technical FAQs

Ask a Question

What are the part number for the control power fuses in the MFLEX enclosed units?

What are the part number for the control power fuses in the MFLEX enclosed units?
Issue: 
What are the part number for the control power fuses in the MFLEX enclosed units?
 
Product Line:
MFLEX Enclosed Altivar 61.71
 
Environment:
MFLEX Enclosed VFD
 
Cause:
Replacement fuses
 
Resolution:
See the attached document for a list of the Primary and secondary control power fuses.            
Helpful Links          
           
The drive MAY be repairable even if parts are no longer available for sale.  Contact Schneider Electric Industrial Repair Service (SEIRS) at 800-950-9550  
Contact your local Schneider Electric distributor for a replacement drive. (search here)  
New!  Try our Drive and SoftStart selection tool for self selection (open style devices)
Technical Support for AC drives and soft starters: 888-SQUARED (888-778-2733) select option 1 for Technical Support and then option 4 for AC Drives and Softstarts.          
Technical Support is available from 8am EST to 8pm EST M-F and 24 hours a day for EMERGENCIES. 
Was this helpful?
What can we do to improve the information ?