Technical FAQs

Ask a Question

What is suffix 4201 for Homeline

Product Line:
HOM-CAFI

Resolution:
The HOM has UL only for the USA market.  The CHOM has CSA only for the Canadian market. 
4201  is a special suffix for HOM that includes both UL and CSA markings. It is avaliable only to select OEM's that do business in both the USA and Canada.
Was this helpful?
What can we do to improve the information ?