Technical FAQs

Ask a Question

What is the capacity of 24 Vdc Power Supply on ATV212?

Issue:
What is the capacity of 24 Vdc Power Supply on ATV212?

Product Line:
ATV21, ATV212, S-Flex

Environment:
All

Cause:
Need to wire external device(s)

Resolution:
24Vdc Power Supply is current-limited to 200mA.
Was this helpful?
What can we do to improve the information ?