Technical FAQs

Ask a Question

When is SoMove scheduled to be compatible with Windows 10?

When is SoMove scheduled to be compatible with Windows 10?
Issue:
Windows 10 compatibility with SoMove.

Product Line:
Altivar Drives

Environment:
All models

Cause:
None

Resolution:
SoMove is not yet compatible nor validated for Win10 - it is expected Q3 2016.
Whatever you do with SoMove on Win10 now, you do on your own risk, without support.
- Customer is probably facing that issue that Modbus driver was not installed automatically.
- It's possible to extract and install manually Modbus driver on Win10 -  please follow the attached below description.
Was this helpful?
What can we do to improve the information ?