Technical FAQs

Ask a Question

After putting the drive in local mode and then back in remote the ATV312 drive is stuck running at 10hz and it will not follow the 4 to 20mA signal.

Issue:
After putting the drive in local mode and then back in remote the ATV312 drive is stuck running at 10hz and it will not follow the 4 to 20mA signal.

Product Line:
Altivar ATV312

Environment:
All

Cause:
Some of the parameters get will reset back to factory default if you go from local to remote.
Resolution:

STEP 1 turn off your preset speeds in reverse order in FUN menu under PSS 
STEP 2 set your LI3 back to NST or freewheel stop or premissive. 
STEP 3 set your FR1 ref 1 back to AI3 in the CTL menu. 
STEP 4 set your two wore type to tct to be level control. 

Programming 
FUN menu enter 
PSS enter preset speeds 
PS4 enter set to NO 
PS2 enter set to NO 
ESC back to PSS 
arrow down to STC enter 
arrow down to nSt enter and program to LI3 

ESC ESC back to FUN arrow up to CTL enter 
FR1 enter set to AI3 enter 

ESC ESC back to CTL menu 
arrow down to IO menu enter' 
arrow down to tCt menu set to LEL 
Was this helpful?
What can we do to improve the information ?