Technical FAQs

Ask a Question

Where can I see the ATV212 power consumption?

Customer wants to see Power consumption from the ATV212 display

Product line:
ATV212, Altivar 212



Using the integral keypad, push the Mode button until you see Fr-F.  This is the Monitoring menu.  Do not push Enter, scroll until you see the following 

H_## - Output Power in kW
h_## - Input Power in kW.  

H## - Total accumulated motor power in kW
h## - Total accumulated input power in kW

# = the numbers detected by the drive.  i.e. h99 is 99kw of total accumulated input power consumed by the drive.  h_99 would be the current input power being consumed by the drive.
Was this helpful?
What can we do to improve the information ?