Technical FAQs

Ask a Question

What is the part number for the circuit breaker of an Econoflex?

Issue:
Circuit breaker part numbers for the Econoflex

Product Line:
Econoflex

Environment:
All models

Cause:
None

Resolution:
The circuit breakers for the Econoflex are listed in Table 38 below.


N/A indicates part is Not Available and was never released for sale.
*FS= Parts are only available from Field Services and require FS installation.
• = Enclosure type - can be “A”, “G”, or “H”. “A"
 
Helpful Links
The drive MAY be repairable even if parts are no longer available for sale.  Contact Schneider Electric Industrial Repair Service (SEIRS) at 800-950-9550
Contact your local Schneider Electric distributor for a replacement drive. (search here)
New!  Try our Drive and Soft Start selection tool for self-selection (open style devices)
Technical Support for AC drives and soft starters: 888-SQUARED (888-778-2733) select option 1 for Technical Support and then option 4 for AC Drives and Soft starts.
 
Was this helpful?
What can we do to improve the information ?