Technical FAQs

Ask a Question

How are the common signal wires connected between the ATV71 and ATV320 drives?

Issue:
Connect common signal wires between two drives.

Product Line:
All ATV71 drives, All ATV320 drives

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
There is a mistake in the ATV320 installation manual.  There is no 0v terminal on the drive, but instead a COM.

For ATV71, the COM and 0V are the same.  So you can connect ATV320 COM terminal  to COM or 0v terminals of the ATV71.

Please note: ATV320 installation manual shows 0v.  There is no 0v on the ATV320, use COM instead.

See attachments
Was this helpful?
What can we do to improve the information ?