Technical FAQs

Ask a Question

What is the Inverter Zero Export function on my ComBox?

Issue:
What is the Inverter Zero Export function on my ComBox?

Product Line:
Conext XW/SW Series

Environment:
Conext ComBox web user interface

Cause:
This feature is not currently discussed in the Owner's Guide for the Conext ComBox

Resolution:
This feature involves a Schneider Electric power meter (such as the PM, EM, or iEM) and the Conext RL grid-tied inverter connected to the ComBox via RS485 Modbus. The ComBox reads the power meter and commands the Conext RL to reduce power if the power meter detects current possibly going to the grid, ensuring zero export. This feature is not compatible with the Conext XW+ or SW inverters, as they are not programmed to accept such a command from the ComBox. However, it will work with a Conext RL that is AC coupled to one of these inverters. Please see the attached document for more information.
Was this helpful?
What can we do to improve the information ?