Technical FAQs

Ask a Question

What is the part number for the NEMA 1 conduit kits for the Altivar 212 drives?

Issue:
Wants to convert the ATV212 drive from Open type (IP20) to NEMA 1 enclosed.  

Product line:
Altivar 212, ATV212

Environment:
all

Cause:
n/a

Resolution:
The open style ATV212 drives are only rated IP00, which is NEMA open type.  By adding the NEMA 1 conduit kit, the drive will become NEMA 1 rated.  See the two attachments for selection, installation and dimensions as needed.  

Noted that ATV212W* part numbers are already consider NEMA 12 enclosed and therefor a conduit kit is not available.  





 
Was this helpful?
What can we do to improve the information ?