Technical FAQs

Ask a Question

What is the master password reset on the ATV630 and ATV930 Process drives?

Issue:
What is the master password reset on the ATV630 and ATV930 Process drives?

Product Line:
Altivar ATV630 and ATV930 Process drives

Environment:
All Models and serial numbers

Cause:
Password has been set and they can not remember the password. 

Resolution:
The master password reset is RESET!  [Note] this will reset your password and your drive back to factory default. If you do not have a copy of the program in your drive please do not reset it back to default otherwise you will need to reprogram the drive by hand. 
Was this helpful?
What can we do to improve the information ?